Hi ,
compare 2 figure
Figure 6. 3-V Firm Overload, Load Stepped from 3.8 A to 5.5 A
and
Figure 7. 3-V Hard Overload, Load Stepped from 3.8 A to 7.1 A
In my view,
Rset = 49.9k, then Iset = 4A,
In figure 6, after OCP, Iload will keep around 3.4A and Vout drop to 2V
In figure 7, after OCP, Iload will keep around 2.4A and Vout drop to 1V
I want to know
1. why figure 6 and figure 7 have different Iload and vout afre OCP.
2. in Equation 4, Vout vary on Ron, is that mean Ron will change in figure 6 and figure 7 ?
is there any Equation can get Iload and Vout in fault time ?