This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PTH12000W: How to find datecode information

Part Number: PTH12000W


Hi, I need to find where I can find the datecode info for this device, i see from the information on the datasheet below it states the device has lot trace code information but i cannot see how i can tie this in to an actual datecode, - I was looking for somewhere online to type the code etc...

(4) There may be additional marking, which relates to the logo, the lot trace code information, or the environmental category on the device.

(5) Multiple Device Markings will be inside parentheses. Only one Device Marking contained in parentheses and separated by a "~" will appear on a device. If a line is indented then it is a continuation of the previous line and the two combined represent the entire Device Marking for that device.

I have a couple of markings from two devices if that helps?

821952V

842132V

Thanks,

  • Nick:

    PTH12000WAH  lot codes(LTC) .manufacturing coding # is located on the power inductor.\

    Lot code  LTC 842132V  is:

    8= Year2018 ,4= month April of 2018, 2132V is the specific TI # assigned  to PTH12000WAH

    LTC 821952V

    8= year 2018 , 2=month February of 2018 , 1952V is the specific TI # assigned  to PTH12000WAH

    Tom