This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65261-1: When input / output capacitors are connected in parallel.

Part Number: TPS65261-1


Hi team.

My customer has inquired about multiple Input/Output capacitors connected in parallel.

Please tell us what problems you may encounter if you use several capacitors with low capacitance instead of one capacitor with high capacitance.

Customers have problems with supply of large size capacitors(MLCC).

For example, two 3216size 100uF capacitors were used for voltage output.

The customer is trying to set this output capacitance to using 1608size 10uF x 20ea.

1. Is there any problem when using several small size capacitors as above?

TI's EVMs have large size and large value capacitors in most cases.

2.  Do you have the information you have tested using multiple small size and small value capacitors in parallel?

Thank you.