This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62150: Inductor Ripple current more than load current

Part Number: TPS62150
Other Parts Discussed in Thread: TPS62147

Hi,

We are planning to use TPS62150 in our design with below specifications.

Input Voltage - 10.5-13.5V

Output Voltage - 3.3V

Output Current - 0.1-0.4A

Based on datasheet recommendation, we have selected 2.5MHz switching frequency and 2.2µH inductor.

Considering 20% tolerance of inductor, maximum input voltage of 13.5V and output voltage of 3.3V, inductor ripple current is calculated using vout / vin x (vinmax-vout) / fsw / L formula as 0.57A. 

Can you please confirm if above ripple current calculation is correct?

In general, we like to keep inductor current within 30% of maximum load current and operate in continuous current mode. However, in this case, ripple current is higher than the maximum load current and hence, a reverse current may flow in the design and/or device may go in dis-continuous mode. Can you please share your comments on this?

Also, is there any alternate part that can be used with above input/output requirements while keeping inductor ripple current below 30% of load current and operating in continuous current mode?

Regards

Raja