Hi,
I believe there is a mistake in the datasheet: Fig. 11 and Fig. 12 are not coherent!
Fig. 11 shows the thresholds for JEITA with threshold voltages for TS pin as proportional to temperature.
However when connecting an NTC as in Fig. 12 the TS voltage will be inversely proportional to temperature!
Indeed, assuming constant VTSB, due to voltage partitioning, TS = VTSB RTH/(RTH+RT1).
Being RTH value inversely proportional to temperature, TS @ 60°C will be lower than TS @ 0°C and vice-versa!
Please clarify ASAP, this looks like a gross huge mistake:
if Fig. 11 is confirmed to work properly NTC and R1 should be exchanged in Fig. 12!
BR,
Vincenzo Fiore