Dear team,
for the TLV704 we are specifying +/-2% at 25°C. Further there is a plot showing typical numbers for -40°C, 25°C and 85°C Vout vs. Vin where you could get some estimate. However we are looking for the max numbers over full temp range -40°C to 125°C. Do we have those numbers? And if so what will be the accuracy over full temp?
many thanks
Lutz