Other Parts Discussed in Thread: BQSTUDIO
hello!
Bq27510-g3 has the following three questions to consult, please help to solve them, thank you!
1:Excuse me, bq27510-g3, when the program selects chemical ID for burning, it prompts an error. Why? As is shown in
2:When creating the Srec file, the error of verification will be prompted. The single can be created successfully. After burning the file into the chip, the chip I2C and BQSTUDIO fail to communicate?
3:When the TS temperature protection of bq27510-g3 chip is not used, is it connected with the pull resistance or the pull resistance?Now we are connecting 1K resistance to the ground. Is that ok?Thank you very much!