I'm using the TPS7A1633DGNR part (8MSOP package) to provide 3.3V in an electric vehicle design where the input can go as high as 60V. The product utilizes a number of LEDs, so the current load can be as high as around 60ma. This is still well below the max for the part of 100ma.
I begin experiencing overheating issues when the input voltage goes as high as 40V. The part begins to cycle on and off and the part gets hot to the touch. It seems to me that the layout provides adequate heatsink copper on the top layer and the grounding is also adequate.
Questions:
1) Can you tell me why the part is getting hot?
2) Would I be better off or worse off using the 8SON part instead?
I have attached layout and schematic pics.
Thanks. Steve