This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Looking for a dual rail power management and charging solution

Other Parts Discussed in Thread: TPS63070, BQ25898D, TPS630252, BQ25898, BQ25890

I am exploring a number of your products and looking to support the following scenario:

Load 1: 5v @2A peak, 1.1A typical

Load 2: 3.3v @1.3A peak, 0.7A typical

Battery powered LI-ION 3.7v 10000mah capacity

Charge in support up to 2.1A

OTG support up to 0.5A

Ability to read battery voltage or optional gas gauge. Currently I am using BQ25898D and 2 TPS63070's but was wondering if there is a better solution.

Thanks,

Larry