This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV741P: Max Output current limit for TLV741P

Part Number: TLV741P


Hi

For TLV741P absolute max output current, TI is internally limited. What does this mean?

what is the spec of the absolute max rating for TLV741P?

  • Hi Tzeh,

    TLV741P has an internal current limit.  Figures 18 and 19 show the typical foldback curve characteristics.  Keep in mind that current limit is a feature to protet against fault conditions only and is not intended to engage under normal operating conditions.  TLV741P was designed, characterized, and tested for a maximum operating current of 150 mA.

    Very Respectfully,

    Ryan