Other Parts Discussed in Thread: UCC27201, LM5102
Hi, my customer is using LM5041. The waveform is as below.
yellow-HD, blue-LD.
Zoom in: they will be both high for 2ns.
They are not sure if it's caused by their circuit problem, or the device itself just act like this.
They use external driver after HD, LD, UCC27201, but this one doesn't have dead time adjustment.
If the device LM5041 act like that, they will need 100V, 3A drive current half bridge gate driver with dead time adjustment, it seems that we don't have such devices.