Hi, all. When I learn the basic knowledge of LDO, I got one question about VDO && VOUT. Whne the output current is the same of TLV73318 and TLV73333, why TLV73333 has a lower VDO? Why VGS voltage is larger in this device?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, all. When I learn the basic knowledge of LDO, I got one question about VDO && VOUT. Whne the output current is the same of TLV73318 and TLV73333, why TLV73333 has a lower VDO? Why VGS voltage is larger in this device?
Hi ,
Please note that TLV733P has a PMOS pass element. Note that the source of the the PMOS is connected to IN for the LDO. In order for an LDO to be in dropout, Vin must approach the nominal Vout. Therefore, a LDO with a lower Vout will need a lower Vin to go into dropout. Since opamp is trying to drive the FET so that the center tap of the feedback resistors is equal to the reference voltage, the gate will be driven to the negative rail of the opamp which is tied to GND. As the gate voltage is 0 V for both LDOs but the lower output TLV73318 requires a lower source voltage to enter dropout, Vgs will be lower for TLV73318.
Very Respectfully,
Ryan