WEBENCH gave me a design which uses the TPS563219 IC as the controller. However, the page says that chip is not recommended for new designs, and suggests using the TPS563219A instead. I checked the datasheets and it seems like the 219A can be used a drop-in replacement for the 219? If not, what is different, so I can change the surrounding circuitry accordingly?