Part Number: BQ24610
Dear experts,I have a question about bq24610's Dynamic Power Management. If I use the bq24610's ACSET Pin to set the total load current as 4A, what will happen when the total current exceed 4A? The bq24610 will limit the input current from external Adapter? When the system load draw 5A, the bq24610 charging current will reduce to 0A and the input current from external Adapter will keep under 4A? Or, the bq24610 charging current will reduce to 0A and the input current from external Adapter will equal to 5A?The bq24610 has current limit functiom? Thanks.