Other Parts Discussed in Thread: TPS7A30, TPS7A47, TPS7A39, PGA2311
Hi,
I'm looking for specific LDO for audio application.
My need:
Regulate a 34V voltage rail to 30V 60mA achieving very low noise
Regulate a 24V voltage rail to 5V 20mA very low noise for PGA23xx component
Regulate a -12V voltage rail to -5V 20mA very low noise for PGA23xx component
I think using the TPS7A49 and TPS7A30 as low noise LDO, is there parts even best especially about psrr ?
I also need a very slow rise time for my 30V voltage rail, about few seconds, says 5 seconds for exemple, is there any issue using a 4.7µF capacitor (with a 10nF in //) as Cnr/ss pin of TPS7A49 device? A such value will give me a soft start about few seconds? How will be the psrr with such a value?
Thanks for support
Florian