Hi,
We are having a issue with the POE part TPS23756 on our boards. The T2P pin on the part is a Active low output that indicates a PSE has performed the IEEE 802.3at type 2 hardware classification. This pin does not go low when connecting to a endspan CISCO Catalyst 2960 even though the Cisco device does detect that our device which has the TPS23756 is Type 2 Class 4 device. We have set the power on the Cisco device to the highest possible of 29W to the device. We do not have this problem with other POE injectors like PowerDSine 9001. Any help would be great.