This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61043: single white LED?

Part Number: TPS61043


Can I use this to drive a single white LED?  

The input voltage in the application will be approx 2V - 3V (two series AAA batteries).

To drive the LED, the output voltage will want to be ~3.5V (3.2V led Vf + 0.25V feedback voltage) so I would roughly estimate the duty cycle to be ~20% when Vin is 3V.  I would assume that the controller can operate at that duty cycle, but I didn't see an indication in the datasheet of minimum switch on-time or duty cycle...