Part Number: UCC27511
Hi,
I am using the model for LTSPice of the UCC27511 gate driver and I have some problems with them, probably because of the ground reference. I am simulating the ANPC topology as you can see in the attached picture with isolated gate drivers where the ground reference is in the middle point. Vdd is 7.2 V with respect the ground of each gate driver that is connected to the respective source of the transistors. However, the PWM pattern is created as shown in the las picture, and they are signals that go from 0V to 5V. If these signals are connected to the input of the respective driver the model does not work. Is there any problem with the PWM reference?
Thank you in advance.
Best regards,
Maria.