This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5041: How to implement remote sensing in Power supply

Part Number: LM5041
Other Parts Discussed in Thread: TL431

Dear friends,

I just want to implement remote sensing in my LM5041 circuit. Can anybody share me the remote sensing circuit diagram?

Regards

Aneesh

  • remote sense.docxH Aneesh,

    I sketched a circuit based on a 5V output for a voltage regulation loop using a 2.5V TL431. The basis of the circuit is that the power connection from Vout + and - to the load will carry the load current and will have a voltage drop due to the series resistance of the wire or PCB track. By using sense connections the voltage drop is eliminated as the sense wires doe not carry the load current and only carry a few mA's of sense current.