Hi
I have some question about the ripple injection for this device.
I think the following circuit(R5,C31,C36) are DNP is the ripple injection circuit. Is that correct?
If it so,
1. How can we calculate the value of the circuit?
(The condition is Vin=12V, Vo=1V, Io=450kHz, L=0.2uH.)
2. Is there any limitation?
3. Also could you advice me if there is any concerns to add the circuit?
Best Regards,
Koji Hamamoto