The TI E2E™ design support forums will undergo maintenance from July 11 to July 13. If you need design support during this time, open a new support request with our customer support center.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27200: Application and Driver for bq27x

Part Number: BQ27200
Other Parts Discussed in Thread: BQ27000, BQEVSW, , BQ27320, BQ27220

Hi,

My customer is looking for the bqEVSW application/driver support for bq27000 and bq27200.  I see that only the Linux driver is available here but no support for windows.  Could you provide the application/driver for these devices?

Thanks,

Chuchen

  • hi Chuchen
    The bq2700 and bq27200 are older legacy devices... is there any reason the customer is staying with this and not migrating over to our new more robust cedv gauges like the bq27320 or the rom counterpart the bq27220?

    WIth regards to the drivers, bqEVSW is what the customer needs to communcate with the device . The can generate a .dfi file using the tool and then write code to program the .dfi file.

    thanks
    Onyx