Our customer cannot write VOUT_COMMAND register.
Their VBOOT setting is 0x5F. After start up, output voltage is 0.72V. This is expected operation.
When they write 0x51 to VOUT_COMMAND register for changing output voltage to 0.65V, the register value is not changed. It is kept 0x5F.
WRITE_PROTECT register value is 0x00.
Is there any cause that we cannot change VOUT_COMMAND register value?
As the same, they cannot write VOUT_MAX register. However it seems like that there is some register which they can write.
We are confirming the register which they can write.
Best Regards,
Kohei Sasaki