Other Parts Discussed in Thread: LM3152
Hello,
It appears to me that the Efficiency of the LM25085 is poor…
Taken from WEBENCH,efficiency is around 70% at 8A.
We can’t proceed with such low performance.
Please advise.
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
The application is small cell base station.
The customer run WEBENCH for the part and got 70% efficiency at 8A,this is poor , why?
He is on the schematic and need fast response other wise he chose competitor.
I suggested him also to test the LM3152, what he need is ,
input: 30v
output: 3.3v
Iout= 10A
Thanks