Hi !
I am as Rodrigo working on a prototype based on the LM5104 working as a switch. The purpose of this montage is to turn on/off a DC voltage (VCC2) going from 1,25 to 7V with a standard 3V3 logic command, knowing that it will mainly remain on.
Here is the associated schematic :
As said earlier, VCC2 can go grom 1.25 to 7Volts, and the VCC supply is 15VDC.
The mosfets used can drive the VCC2 voltage without trouble, but have a low VGSmax. That is why there are voltage dividers on both HO and LO command outputs.
The montage works as expected, meaning that the output LS_EN can be turned on and off for all VCC2 values, but for some reason several LM5104 burned while trying this montage. Is there something in that configuration that could lead to a failure of this chip ?
Regards,
Léo