This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3481: Buck-boost using SEPIC

Guru 16770 points

Part Number: LM3481

Hi

1.

Is it possible to satisfy following requirement using LM34381 SEPIC operation?

Input:3V-4.2V

Output:3V-8.5V

Output current:1.3A

2.

Is it possible to modify LM3481SEPICEVAL to satisfy our requirement?

BestRegards