This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24780S: Input current limit setting to support hybrid power boost mode

Part Number: BQ24780S


Hi,

From section 7.4.2 Hybrid Power Boost Mode in datasheet, I understand that the input current limit setting must be higher than 1536mA to support hybrid power boost mode. It means that hybrid power boost mode does not work when input current is higher than 107% but IINLIM is less than 1536mA. Is my understanding correct?

Best Regards,

Satoshi / Japan Disty