This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25120A: BQ25120A performance at 12V

Part Number: BQ25120A
Other Parts Discussed in Thread: BQ25120, LM2840

Hello,

I have been looking at the datasheet of BQ25120A  to evaluate whether it can be used to recharge a Li ion cell when powered from a 12V vehicle battery. The IC seems to have been optimised for 5V operation. Is this IC meant for use with a constant 12V input ? If so, is there any data that can be referred to?

Thanks,