Hi,
thanks for the answers.
About the inductor, do you think that WE 74485540101 or SRF1280A-8R2Y could be a right choice? From my calculations, for uncoupled inductance, the min value is 9.3 uH, ΔIL = 2.4 A and IL(peak) 7.5 A. If not, can you suggest me a suitable inductance?
Equation 10 refers only to MOSFET power dissipation, so any choice of MOSFET is right if it can dissipate this power; but, I suppose that, increasing the Total Gate Gharge, at a specific switching frequency, it is required more power to drive the mosfet. LM3478 has to provide this power, that can't be limitless, and none information are in the datasheet or in the application note about this; unless you're telling me that, under any capacitive load and frequency conditions, LM3478 automatically limits the power supplied via the DR pin to avoid overheating.
About trouble 4, I've further investigate it. The problem doesn't depend by the input voltage, but by the input current. Limiting the input current, under a specific value at a specific input voltage (for example 20 V, 2 A), the regulator fails to reach the proper output voltage, also without load, because, at the power on, the regulator drains all input current, the input voltage falls (at 4 V in the example) and the output voltage is instable (between 6 and 10 V). In this condition, the gate voltage is almost constant and equal to the input voltage, so all the input current flows in the inductor and in the mosfet.
Could not this be a problem?
I've solved trouble 5 adjusting compensation filter.
Thanks for your help