Hello,
Does anyone know if this part can be used in applications requiring 60601 or 60950 requirements? I'm no expert, but the pin spacing is only 0.25mm or so, which seems like it wouldn't meet creepage and clearance requirements. The datasheet states "Promotes Safety in Medical Equipment" but nothing about being compliant to the standards.
My understanding (for my 5V charging system):
Clearance:
60601: 1mm (1 MOPP)
60950: 0.4mm
Creepage:
60601: 2mm (1 MOPP)
60950: 1.1mm
Thanks,