Part Number: BQ25504
Hi Sir,
Sorry about old question has been closed. I open new question for this topic.
We finally increased the CSTOR in system (CE1) to 470 uF. It seems resolved the question. However when we increased the charger power, it has failed.
In old question, we can not see VBAT traces VSTOR. That's why we were concerned about this question.
We used the 14500 800mAH Li ion rechargeable battery in this system, we cannot provide scope capture of the charger behavior when battery is more than 3.5V (VBAT_OK_HYST) to 4.22V (VBAT_OV).
The battery need 3 days to be recharged 0.1 Volt.
Our question still can be described as below picture.
Yello: +VSTOR
Blue: +VBAT (3.146V Li-On Battery)
Purple: VBAT_OK
When +VSTOR rises to VBAT_UV, the internal PMOS will be opened. The +VSTOR and +VBAT will be the same, right?
However our system will raises the VBAT_OK to open external PMOS. Does it seem that skip the charger mode?