This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC27524: Recommended Output Resistance and Bypass Capacitance

Part Number: UCC27524

I'm planning on using this chip for 2 different applications to drive GaNFETs. Below are the specs for each:

1 - 

Vin: 3.3 V

Vout: 5 V

Ids: 2.8 A (Max)

2 - 

Vin: 7.5 V

Vout: 5 V

Ids: 2.8 A (Max)

What would be the ideal output resistor value be for the UCC27524, and is there a recommended bypass cap value? I was thinking of using a 0.1uF and a 10uF.