I'm going through the datasheet for the LM5088 trying to estimate values for the various parts required. The formula in Section 9.4.2 to calculate the Inductor value uses Vin(max) and of course I'm confused as to what value I'd use for that. On the face of it it's a 12V automotive system but when the engine is on and charging I'd expect the Voltage of the system to be about 14.5Volts. Lets say 15V to keep with nice round numbers. So I've got 15V as the maximum input voltage.
But hold on a minute the only reason I'm here is I'm trying to power a 5V uC board in an environment which will potentially have load dumps forcing the input voltage to spike up to 100V perhaps even 150V so is that the maximum voltage I should be putting into the formula.
Actually am I even looking at the right part here? Is there a better DC/DC converter which will cope with automotive load dump and inductive loads