Part Number: UCC28951-Q1
Other Parts Discussed in Thread: UCC28950
Hello Team,
Please tell me about the following two items for UCC28951-Q1 used as SLAVE mode with external clock.
According to SLUS609 application note written for UCC28950, family device in the same application;
1. The pulse width of external clock signal to Sync-pin has been needed as >300ns.
Is this 300ns _min applied to both logic "high" and "low "regardless of frequency for UCC28951-Q1?
2. External clock to SYNC pin should need the frequency over x1.8 of internal frequency set by RT resister.
If internal frequency has +/-15kHz variation as 100kHz_typ, How is estimated the minimum frequency of external clock?
Is 207kHz(=115kHz*1.8) needed as minimum frequency? or is 180kHz(100kHz_typ*1.8) is enough?
Best regards,
Hidekazu Someno