Hello,
I have a OMAP3530 board similar to the EVM on which the MMC/SD card detect goes to the TPS69520 GPIO1. With no card inserted, I see the card detect line go low about 10 times a second. I assume that the Linux driver is responsible, but is it possible that there's a significant difference in the configuration registers between the EVM TWL4030 power IC (for which I could not find docs) and the TPS69520 which might cause this behavior?
Thanks,
John