Other Parts Discussed in Thread: BQ24192
I'm using the bq27531-g1 + bq24192 solution to manage the battery .
In the user's guide,it requires to use an external NTC 103AT-type(10KΩ) thermistor to measure the temperature of battery.
(the temp measure via on-chip temp sensor is out of consideration, because the temp might be different between chip and battery)
However, I'm using a battery with an NTC thermistor of 47KΩ, is there a solution that I can mersure the temperature without replacing the NTC thermistor?