This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR14030-Q1: Max Frequency Setting

Part Number: LMR14030-Q1

Hi, team.

The frequency setting range of the LMR14030-Q1 is specified as 2.5 MHz as the maximum.

But does it need to be within 2.5 MHz considering the deviation of the set frequency and the shift due to the frequency spread function?

Or if the set value is 2.5 MHz, is it OK to somewhat exceed?

Best Regards,