Hello,
I am using BQ24171RGYT with a pack of 18650 LiPo cells in 3P2S configuration (7.2V).
Problem: Precharge phase seems to get skipped. Charge starts are programmed current of 4A. Datasheet says precharge should limit initial current to Icharge/10 = 0.4A for 30 minutes but that does not seem to happen.
Test Steps: This happens on at least 2 sets of professionally built HW. Plug in battery, plug in external power supply, measure battery current = 4A.
HW:
R1 = 300KΩ
R2 = 95.3KΩ
Rsr = 0.01Ω
Calculations:
Viset_calculated = Vref (R2 / (R1 + R2) = 3.3 (95300 / (95300 + 300000)) = 0.80V
Viset_measured = 0.78V.
Icharge = Viset / (20 x R_sr) = 0.78 / (20 x 0.01) = 4A
Results:
Since Viset_measured is similar to calculated value, I assume my divider resistors are correct. Not sure what else to check.
Question:
Has anyone experienced this? Any idea what could cause it?
Thanks for any help.