This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62671: TPS62671 EVM evaluation

Part Number: TPS62671
Other Parts Discussed in Thread: TPS62821, TPS62801, TPS62088

Dear ,

Do we have evaluation board for TPS62671, and can I apply for one for our customer?

Thanks.

  • Hello John,

    for this product you need to use a pin to pin compatible EVM and mount a sample of the TPS62671. I would suggest this one:

    If I may give you a further suggestion, there are a bunch of newer products with better performances. In common those devices have very low IQ (4uA or less). In particular:

    TPS62821: 2x1.5mmm QFN package, 1% Vref accuracy in the whole temp range -40 to 125 degC, 470nH inductor.  

    TPS62801: 1.05x0.7x0.4 mm WCSP package, 1% Vref accuracy,  470nH inductor, Output Voltage selection pin.  

    TPS62088: 1.2x0.8 mm WCSP package, 1% Vref accuracy,  240nH inductor, Fixed Output Voltage versions.  

    For all of these you can find a dedicated EVM, Webench and PSpice model to support you and your customer in the design process.