Hi all,
I have been working with BQ24105 and i have connected to the TS pin a thermistor NTC 103AT (the same reported to datasheet and EVM). I have designed the network RT1, RT2 in order to get a temperature range from 0 to 45C using the formulas treported at page 14 of datasheet and I have got RT1 9.31K and RT2442K (the same of datasheet) but I got a completly different temperature range. The effective temperature range is 20 to 90C. The voltage on VTSB pin is 3.15V. Can you give me some ideas?
Thanks a lot