Hi
There is the maximum duty on the datasheet. However it is only for Rfreq=80kohm.
How much is the duty max when it is for Rfreq=22.9kohm(2MHz)?
If the duty max decrease with increasing the frequency, is the off time fixed for this device?
In my experience, the duty max decrease with increasing the frequency.
However the off time at each frequency is not same. (At faster frequency,the off time is shorter.) How does the off time define in that case?
Best Regards,
Koji Hamamoto