Other Parts Discussed in Thread: TPS92518
I'm using the TPS92518 Evaluation Board to test the linearity of the part. I'm trying to conduct efficiency tests to determine what kind of real numbers would be used in the equations to better predict the value for t(off).
I'm testing at maximum voltage at the moment and to get the target frequency I desire, 800 KHz, I need to set LEDx_TOFF_DAC to a number less than 10, but the software won't let me. It changes any number less than 10 to 10. If I set it to 10, the frequency I get is just over 500 KHz which is not fast enough to meet my ripple requirements or to test efficiency in a low head room condition.
Is there a way to make the software set LEDx_TOFF_DAC to less than 10?
Thanks.