Other Parts Discussed in Thread: UCC28180
Hi
Can you help with below several questions for UCC28070A from my customer?
- Open‑Loop Detection
- Datasheet mentioned open-loop detection, however there is no detailed description about this function in datasheet. Can you help to elaborate on this?
- How should I connect CSA,CSB if I only need one-phase instead of two-phase interleaved?
- See below line highlighted in red, does it mean if I connect RSYNTH to VREF, the CSA and CSB will automatically connect to respective current amplifiers?

- What specifically does this falling percentage mean? Does it mean that output voltage should drop at around 93% to trigger slew-rate correction?

- What does this parameter(phase mismatch) refer to? Can you help with more details?

Many thanks in advance!