Hello,
we want to use an LP8556 in our design and have two questiosn about it, i hope i can get help here.
For the package type there are 3 different Devices given. LED Channel Count 5,4, or 6.
Which channels are useable in which part? There is no description which of the 6 channels are lost in the 4 and 5 channel devices.
Under device option is written „PWM ONLY“ – Recommended for Systems without an I2C master. So I2C cannot be used for these devices?
Or is a communication between a master and the LP8556 via I2C always possible and i have to change a register, so i can use I2C instead of PWM to controll the backlight?
I really hoope there is an easy answer for these two questions.
Best regards,
Thomas