This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5008AEVAL: Strange SW waveform

Part Number: LM5008AEVAL


Just test the LM5008AEVM and find that the SW waveform is not so "standard" at the begining of HS MOS on phase.  It will happen once the input voltage exceeds 50V. Why? SW waveform is attached.

Input: 80V. Output: 5V, 200mA