This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27510: Charging / Discharging current is not correct even after calibration

Part Number: BQ27510

Hi all, 

We are using BQ27510 as battery monitor in one of our designs. 
We are using EV2300 for communicating with the BQ27510 for initial development. 
Initially everything worked as expected & we were able to read proper voltage & current from the battery monitor. 

During initial configuration, by mistake IT_Enable command was sent & after this the battery charging / discharging current is not accurate even after the calibration. 
Battery monitor shows 140mA charging current even when there is no load / charger connected to the system. Any load or charging current is added on top of this 140mA.
It seems like there is a offset error of 140mA & this is not corrected even after CC offset / Gain or Charging current calibration.

We tried Reset command to reset the entire battery Monitor & also uploaded the default firmware.
But above things have not resolved the issue. 
I have attached the .gg file for your reference. 

Please suggest the possible reasons / ways to resolve this issue. 
Looking forward to valuable suggestions. 

/cfs-file/__key/communityserver-discussions-components-files/196/5658.Data_5F00_Flash.gg.zip

Thanks,

Suresha