This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MOSFET Gate driver selection

Other Parts Discussed in Thread: UCC21222-Q1, UCC21520-Q1

Need to select a proven driver in terms of adoption in the Industry.

Specs are as follows.

 

Its basically a Half bridge driver.

 

DC link voltage : >100V

Driver Ouput Current rating >2 Amp

Input Voltage compatibility 3.3V/5V

Driver Enable pin : Required

Dead time control : Required (Variable or fixed)

Number of input pulses : Hin and Lin or Single input

Maximum driver voltage : >15V

Isolation :    Required

Qualification : AEC