This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/TPS61093: Using 500mA case

Part Number: TPS61093
Other Parts Discussed in Thread: TPS61085

Tool/software: WEBENCH® Design Tools

Hi,

We is thinking about using this device below condition.
Vin:5V
Vout:8V
Iout:0.5A

But this device has Overload protection. This threshold value is Typ 300mA.
WEBENCH outputted below circuit at this condition.
I think this device can not use this condition because current value hits overload protection.
Is it correct?


Best regards,
Shimizu