This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS92602-Q1: PWM dimming light LED very slow

Part Number: TPS92602-Q1

I am trying to use PWM dimming to light 15 LED on TPS92602 EVM. My input voltage is 19V and output 0.06V to  ICTRL pin then I output 1/100 duty PWM signal to light LED. After about 2 ~ 3 seconds, LED start to light up slowly. I don't want to wait 2 ~ 3 seconds the LED start to light up. I want LED light up immediately when I output PWM signal. How do I do ?

Thanks

Janson