I'm curious as to the reason for the specified 10uF output capacitance limit. Is this really a stability issue, or just the range of capacitance that was used for design simulations? I'd like to use 2 x 10uF 6.3uF X5R caps on the 1.8V output. Under bias the capacitance will be less than 20uF, but likely more than 10uF. Please advise on what problems might be seen or if I'm in the clear.