Tool/software: WEBENCH® Design Tools
I want to use TPS54531 ic for an output of 5V,5A. My Vin minimum is 5V and Vin maximum is 7.4V. But when I give these values in WEBENCH tool it didn,t show any parts for this design. The TPS54531 has an input range of 3.5V to 28V and 5A output current range. Is this the problem of WEBENCH tool or is there any major problems with my design values or my part selection?